Browse FAQs

Is SYMax Programming software still available?

Published date: 26 June 2020

Issue:
Software for Sy/Max product

Product line:
Sy/Max

Environment:
Winmate SFW572

Cause:
No software to connect to the PLC.

Resolution:

The WinMate programming software, ordering part number 8010SFW572 can still be ordered through the Service Sales group. Simply send an email request to "service.sales@se.com" and ask for pricing and availability on the WinMate 8010SFW572 programming software.

For the programming cable, NR&D sells a SC902 Smart cable which is a SyMax compatible RS-422 cable with a miniature RS-232/RS-422 converter built into the 9-pin RS-232 end. It is intended to be used to connect the 9-pin RS-232 COM port of a personal computer directly to the SyMax compatible RS-422 port of the controller. To purchase the SC902 cable contact to NR&D (Niobrara Research & Development) at #800-235-6723.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.