Browse FAQs

What can I use a gateway between Ethernet TCP/IP to Modbus for an ATV312 drive for?

Published date: 15 June 2020

Issue:
Ethernet TCP/IP to Modbus gateway

Product Line:
ATV312, ATV31

Environment:
All models and serial numbers

Cause:
None

Resolution:
Both EGX100SD and TSXETG100 can be used. The EGX100SD is rated at a higher temperature for when used in an enclosed panel. The TSXETG100 is for an open style.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.