Browse FAQs

What is the power or current draw of Powerlink Power Supply?

Published date: 24 June 2020

Issue:
What is the power or current draw of Powerlink Power Supply?

Product Line:
Powerlink G3 Lighing Control

Environment:
Lighting Control

Cause:
Project has a Line Feed 120 V Power Supply (NF120PSG3L).  Electrician wants to verify that he is feeding it correctly.

Resolution:
The Power Supply draws 20 VA max. 
At 120 V, it will draw 0.167 A.
At 277 V, it will draw 0.072 A

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.