Browse FAQs

What could have caused the error: "Application has halted. Not enough memory for initialization procedure. IVM:object.c: Line1823." when going into Web Gate over the internet through a router?

Published date: 26 June 2020

 Issue:
What could have caused the error: "Application has halted. Not enough memory for initialization procedure. IVM:object.c: Line1823."  when going into Web Gate over the internet through a router?
 
Product Line:
Vijeo Designer, Magelis, Web Gate, Webgate
 
Resolution:
It could be that the Magelis did not have a Gateway IP Address.  Please add a gateway address and the error goes away.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.