Browse FAQs

Database Manager Archive fails - Could not deploy package

Published date: 26 June 2020

Issue
When attempting to archive in Database Manager, the following error occurs: 

The following error occurred:
An error occurred while executing SqlPackage: *** Could not deploy package.
Missing values for the following SqlCmd variables:LogFilePath.




Product Line
ION Enterprise
Struxureware Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x

Environment
Database Manager Archive

Cause
Issue is caused when attempting to save the archive to the root directory of the hard drive.

Example:
"C:\ION_Data_Archive14_08_20_11_05"


Resolution
Change the "Save archive to" to include at least one sub folder within the root directory. 

Example:
"C:\DatabaseArchives\ION_Data_Archive14_08_20_11_05"

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.