Browse FAQs

What is the difference between EM4000 and EM4800 Series Meters?

Published date: 29 June 2020

Issue:
A user requires to know the difference between the EM4000 and EM4800 Series Meters in order to select the appropriate Powerlogic EM4X00 Model.
 
Product Line:
EM4800, EM4805, EM4833, EM4880
EM4000, EM4033, EM4080
 
Environment:
Feature and Capability, Comparison
 
Cause:
The products are almost identical. User is unable to identify the difference between the EM4000 and EM4800 Series in order to make a selection to purchase. 
 
Resolution:
There are only two differences between EM4000 and EM4800 Series meters:
1) EM4800 Series meters are Measurement Canada approved.
2) EM4800 Series meters have a Modem Port. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.