Browse FAQs

What are the dimensions of the mounting plate of the remote mount kit part number VW3A1102?

Published date: 15 June 2020

Issue:
Dimensions for mounting plate in the remote mount kit part number VW3A1102

Product Line:
ATV61, ATV71, ATV312, ATV212

Environment:
All Models and Serial numbers

Cause:
None

Resolution:
W=105mm  /4.53in
H=116mm  / 4.57in
D=<03mm   / 0.12in

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.