Browse FAQs

Does Square D offer a generator interlock kit for the 400amp QO load centers(QONQ42MS300, QONQ42MS400, QONQ30LS400 and QONQ42LS400)?

Published date: 05 June 2020

Issue:
Product Design Features 

Product Line:
QO Load Center

Environment:
400A Load Centers

Cause:
Generator interlock kits

Resolution:
There is NO generator interlock kit available for the 400A, QO load centers. Generator interlock kits are only available for load centers rated up to 225A maximum.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.