Browse FAQs

Can Short Circuit Protection be disabled on the Altivar 61 / Altivar 71 series drives?

Published date: 15 June 2020

Issue:
Wanting to disable the Short Circuit Protection on the Altivar 61 / Altivar 71 series drives.

Product Line:
Altivar 61 / Altivar 71 series drives.

Environment:
All models, All serial numbers.

Cause:
Clarification of Short Circuit function is needed.

Resolution:
Short Circuit Detection is always enabled in the ATV61 / ATV71 series drive.  Short circuit fault detection is a hardware based detection system, not software. There are no parameters that can be adjusted to disable this protection.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.