Browse FAQs

What is the part number for the ATV61 and ATV71 main control board flash kit?

Published date: 24 June 2020

Issue:
ATV61 and ATV71 main control board flash kit part number.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs a flash kit to update the main control board.

Resolution:
The ATV61 and ATV71 flash kit part number is VW3A9703.  This part can only be ordered through local Field Services.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.