Browse FAQs

When did the ATV16 Drive become obsolete?

Published date: 17 June 2020

Issue:
ATV16 obsolescence

Product line:
ATV16, Altivar 16

Environment:
All models.

Cause:
Determine age of unit, product obsolescence

Resolution:
The ATV16 became obsolete in 1996. The current replacement is the ATV12 or ATV320, depending on the application. There are some differences that should be reviewed by the customer such as wiring, dimensions, and ratings.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.