Browse FAQs

Wiser Thermostat EER58000 does not keep the setpoint that I set.

Published date: 05 June 2020

Issue:
Wiser Thermostat does not keep the setpoint that I set. 

Product Line:
Wiser Home Management System

Environment:
North America, Residential Home

Cause:
If not connected to a Wiser Network, the factory default programming of the thermostat is to follow a pre-programmed temperature schedule.  If one adjusts temperature with the Up/Down buttons, then the themostat will be in Manual Mode.  It will only hold that temperature until the next time period.  That next schedule time period boundary, the thermostat will go back to the setpoint temperatures set by the schedule 

Resolution:
In order to hold the temperature indefinitely, set the Hold Mode to "Away."    When you return to the main screen, it will say "Hold" on the left side of the screen. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.