Browse FAQs

What size wire gauge should be used for Powerlink G3 input terminals?

Published date: 05 June 2020

Issue:
What size wire gauge should be used for Powerlink G3 input terminals?

Product Line:
Powerlink G3 Lighting Control

Environment:
North America, commercial lighting control

Cause:
information about wining of input terminals

Resolution:
18 AWG is the recommended wire size.  Wire connector can accomodate 14 to 28 AWG, but 18 is recommended.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.