Browse FAQs

Can the ATS48 delay starting the motor after a run command is given?

Published date: 17 June 2020

Issue:
Wondering if you can use the  ATS48 and delay running the motor after the run command is given?

Product Line:
ATS48 Altistart 48

Environment:
All

Cause:
Need time delay after run command

Resolution:
No, the ATS48 does not have a setting to delay the motor start after the run command is given.  Such a function needs to be done in the control circuit to delay the run command to the ATS48.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.