Browse FAQs

What control voltage is needed for an ATS01N2..LY?

Published date: 24 June 2020

Issue;
control voltage needed for an ATS01N2..LY

Product Line:
ATS01

Environment:
ATS01N2..LY

Cause:
Control power required on terminals 06-07.

Resolution:
The control power applied to terminals 06-07 is specified at 110Vac +-10%, 20VA.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.