Browse FAQs

What can cause an Max Sensor fault on the ATV61 Walmart drive?

Published date: 20 July 2020

Issue:
Max Sensor fault on Walmart's ATV61.

Product Line:
Altivar 61 Eflex at Walmart Stores only

Environment:
Walmart Stores that are using the Eflex enclosed drives

Cause:
The ambient temperature or the pressure transducer is maxed out or has faulted.

Resolution:
The Max Temp fault accrues when either the Temperature or Pressure sensor has maxed out its range for 15 mins.   Go into menu 1.14 of the drives programming menu and check the ambient temp value.  If its cold outside and the ambient temp is reading  140 degrees F  then is a good chance the sensor might be bad.



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.