Browse FAQs

Where do you find Short Circuit Current Ratings (SCCR) and branch circuit protection information for ATV32 drives?

Published date: 22 June 2020

Issue:
ATV32 drive Short Circuit Current Ratings (SCCR) and branch circuit protection information

Product Line:
Altivar32, ATV32

Environment:
All

Cause:
Add extra protection at the line of the drive.  Meeting certain UL ratings. 

Resolution:
Attached combinations in the table have been tested per UL508C. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.