Browse FAQs

Power cycled the HMISCU and getting the message: "the codesys runtime has stopped". How to put the controller into Run?

Published date: 29 June 2020

Issue:
Power cycled the HMISCU and getting the message: "the codesys runtime has stopped".  How to put the controller into Run?

Product Line:
HMISCU, Somachine

Environment:


Cause:


Resolution:
There is no Run input for the HMISCU combo units.  You will need to create an external variable with an address of @Prop:0 in Vijeo Designer.  Then create an Action on start up to write a value of "1" to that external variable.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.