Browse FAQs

How to convert a Magelis Codesys project into a M258/M241/M251 Somachine controller?

Published date: 26 June 2020

Issue:
How to convert a Magelis Codesys project into a M258/M241/M251 Somachine controller?

Product Line:
Magelis, Codesys, Somachine, M258, M241. M251

Environment:


Cause:


Resolution:
The way to convert a Codesys application from a Magelis to Somachine controller is by doing the following.

1 - Export the POUs, GVLs, Functions, Structures by going to the Project Menu -> select Export.
2 - A window will pop up, select the POUs, GVLs, Functions, Structures, etc.. that you want to bring in to the Somachine controller.  It will create a *.export file.
3 - Create a new project with the Somachine controller and import the *.export file by going to the Project Menu -> select Import and select the *.export file.
4 - Follow the Import wizard to complete the import.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.