Browse FAQs

What is the master password for the ATV61 and ATV71 drives?

Published date: 14 May 2020

Issue:
Master password for ATV61/71 drives?

Product Line:
Altivar ATV61 and ATV71 drives

Environment:
All

Cause:
Customer does not know the password and would like to bypass it to make a simple programming change

Resolution:
There are two pin codes that can be set on the ATV61 and ATV71 drives.
From the Main Menu scroll down to 'Password' and press Enter
Pin code 1 password reset is 6969
Pin code 2 password reset is 2663
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.