{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Schneider Electric USA Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Search FAQs

What is the SNMP capability for Schneider Electric PLCs?

Issue:
Transparent Ready products that support SNMP
 
Product Line:
Modicon Quantum, M340, M580
 
Environment:
Unity
 
Cause:
N/A
 
Resolution:
 Schneider Electric Transparent Ready products support two SNMP MIBs:
Standard MIB II: This first level of network management can be accessed via this interface. It lets the manager identify the devices that create the architecture and retrieve general information on the configuration and operation of the Ethernet TCP/IP interface.

MIB Transparent Ready interface: Schneider has obtained a private MIB, groupe_schneider (3833) (see page 355). This MIB includes a set of data that enables the network management system to supervise the Ethernet services. The Transparent Ready private MIB can be downloaded from the Web server on any Transparent Ready module in a PLC.

SNMP is used to do the following:
1. query devices, such as host computer(s), routers, switches, and bridges, to determine their status
2. obtain statistics about the networks to which they are attached
Explore more

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.
Explore more