Browse FAQs

Video: How to determine which option card is installed on the ATV61 or 71 drives?

Published date: 18 June 2020

Issue: 
Determining which option card is installed on the ATV61 or 71 drives.
 
Product Line:
Altivar 61, Altivar 71
 
Environment:
All Serial numbers
 
Resolution:
To determine if an option card is installed on the ATV61/71, go to menu 1.11 in the drives menu enter and find menu option 1 and option 2 this will display the option cards installed.



Troubleshooting tips:
If one of the options 1 or options 2 show an unknown option or if unknown is displayed, check the card to see if it's seated correctly or try reseating the option card.
If there is problem with one of the option cards and you need to get the part number of the option card that is installed, you can find the VW3AXXXXX part number on the white bar code on the leg of the option card.
See the image below.




See the attached ATV61 Installation Manual for further details. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.