Browse FAQs

Can I use an encoder on an ATV32?

Published date: 24 June 2020

Issue:
Wants to use an encoder on an ATV32.

Product Line:
ATV32

Environment:
All products of ATV32

Cause:
N/A

Resolution:
No, the ATV32 has an encoder option VW3A3620 for speed regulation only.  It does not do closed loop functionality with the encoder.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.