Browse FAQs

What is the best motor control type to use for fan applications on ATV71 drives?

Published date: 24 June 2020

Issue:
Recommended ontrol type for constant torque fan application on the ATV71 drive

Product Line:
Altivar ATV71

Environment:
All

Cause:
Wants to know if he needs to change the motor control type.

Resolution:
Normaly, lower duty application best run with V/F 2 points setting.  The default setting is SVCV.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.