Browse FAQs

Can rpm (motor rated speed) be set on an Altistart Soft starter?

Published date: 24 June 2020

Issue:
RPM setup on an Altistart Soft starter

Product Line:
Altistart Soft starters

Environment:
All serial numbers for Soft starters

Cause:
N/A

Resolution:
No it cannot. Unlike an Altivar Drive, the soft starters do not have any control of the motor's speed. So there no need to include the rpm ratings in the soft starter.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.