Browse FAQs

What is the MTBF for 140CPU67861 in hours ?

Published date: 20 June 2020

Here is the MTBF figures in hours at different temp and continuous operation.

140CPU67861                   
Mtbf 30° Continuous operation
750944.688

Mtbf 60° Continuous operation
437005.446

Mtbf 85°C Continuous operation
259608.23

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.