Browse FAQs

What is Profile on the ATV61/71?

Published date: 20 June 2020

Issue: 
ATV61/71 Profile.
 
Product Line:
Altivar 61, Altivar 71
 
Environment:
All serial numbers
 
Cause:
N/A
 
Resolution:
The behavior of the Altivar 61 can be adapted according to requirements:
• [8 serie] (SE8): To replace an Altivar 58. See the Migration Manual.
• [Not separ.] (SIM): Command and reference are sent via the same channel.
• [Separate] (SEP): Command and reference may be sent via different channels.
In these configurations, control via the communication bus is performed in accordance with the DRIVECOM standard with only 5 freelyassignable bits (see Communication Parameters Manual). The application functions cannot be accessed via the communication interface.
• [I/O profile] (IO): Command and reference may be sent via different channels. This configuration both simplifies and extends use via
the communication interface.
Commands may be sent via the logic inputs on the terminals or via the communication bus.
When commands are sent via a bus, they are available on a word, which acts as virtual terminals containing only logic inputs.
Application functions can be assigned to the bits in this word. More than one function can be assigned to the same bit.
Note: Stop commands from the terminals remain active even if the terminals are not the active command channel.
Note: The integrated Modbus channel has 2 physical communication ports:
- The Modbus network port
- The Modbus HMI port
The drive does not differentiate between these two ports, but recognizes the graphic display terminal irrespective of the port to
which it is connected.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.