Browse FAQs

What are the dimensions of an HCM64TFD?

Published date: 02 June 2020

Issue:  
Need to know the size of HCM64TFD trim

Product Line:
I Line panelboard enclosure cover / trim.

Environment:  
US product line

Cause:
Dimensions

Resolution:  
Per catalog 2110CT9701, page 17, the dimensions for the flush cover are 66" H x 34.25" W, standard dimensions of the enclosure are 64" x 32".

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.