Browse FAQs

What is the 004 suffix on the 450R-120-004 Voltage Transformer?

Published date: 11 June 2020

Issue:
What does the 004 suffix on the 450R-120-004 Voltage Transformer mean?
 
Product Line:
Voltage Transformer
 
Environment:
Instrument 600 Volt Class Transformer
 
Cause:
Customer is needing a replacement or cross for the 450R-120-004 voltge transformer.
 
Resolution:
The 450R-120-004 had a "tapped primary" of 120 / 69.4.   This part number is no longer available.
If you application does not require the taps you may consider the 450R120. It is without any taps (2 wires in and 2 wires out).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.