Browse FAQs

What adjustments have to be made if you want to run the ATV71 drives on a centrifugal water pump?

Published date: 24 June 2020

Issue:
Adjustments to run an ATV71 on a centrifugal water pump

Product Line:
Altivar ATV71

Environment:
All 

Cause:
Wants to set up the Altivar ATV71 drive to run a basic water pump. 

Resolution:
Set up all of you motor name plate data in menu 1.4 motor control or in menu 1.1 simply start menu.
Then set your motor control type in the Menu 1.4 motor control menu to VF 2 Points. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.