Browse FAQs

Can 30hp or larger, 480v IEC starters be offered in a Model 6 MCC ?

Published date: 05 June 2020

Issue:
What size of IEC starters can be used in MCC Model 6

Product Line:
Motor Control Center

Environment:
Model 6

Cause:
High Density units

Resolution:
Our MCC6 will only take up to a 25hp, 480v starter . We offer a TMD2 (MCC6) in Canada and that can take larger IEC sizes. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.