Browse FAQs

Are the bolts on LGF36600U31X captive?

Published date: 28 June 2018

Issue:
Bolts on LGF36600U31.

Product Line:
Circuit Breaker

Environment:
PowerPact L-Frame Breaker

Resolution:
The terminal screws are tightened to 50Nm or 442 lb-in and can be removed if required. The lug cover should be removed first in order to remove the terminal screws.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.