Browse FAQs

What are the Module part numbers for a ​TVS3EMA24AIC SPD?

Published date: 11 June 2020

Issue:
What are the replacement part numbers for a ​TVS3EMA24AIC SPD?

Product Line:
TVSS Surge Protective Devices

Environment:
Maintenance

Cause:
Replacement

Resolution:
The TVS3EMA24AIC SPD is a 240V B High leg Surge protective device with a B phase module , rated for 208V , on a high leg systems.
The replacement module is different than the A and C phase modules.
The B phase replacement module is p/n MA3IMA24 , with A and C phase modules (120V) , p/n MA1IMA24.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.