Browse FAQs

The Q frame part numbers with F, M, and P termination options do not show as valid numbers.

Published date: 19 June 2020

Issue:
The Q frame part numbers with F, M, and P termination options do not show as valid numbers; Are Q frame breakers only available as lug-in/lug-out and I-line configuration?
 
Product Line:
Powerpact Q-frame Circuit Breakers
 
Resolution:
The Q-frame breakers, when used with these termination options, also require suffixes indicating the studs. The options are as follows:

When using termination option F, suffix -TS must also be added (ie. QBF22200TS).
When using termination option M, suffix -TN must also be added (ie. QBM22200TN).
When using termination option P, there are two options: with suffix -TM, the studs will also be installed with nuts and washers added (ie. QBP22200TM), or with suffix -TP, the studs will be installed and the nuts and washers will be supplied separately in a bag (ie. QBP22200TP).

See attachment for graphic of catalog numbering system for Powerpact Q frame breakers.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.