Browse FAQs

What is the SCR test procedure for the RAM DBS II starter?

Published date: 01 June 2020

Issue:
SCR test procedure for the RAM DBS II starter

Product Line:
DBS and DBS II

Environment:
All models

Cause:
Test the SCR integrity

Resolution:
Please note that the DBS and DBS II product lines were sold to Indicon Corp.
Technical support contacts:
Leesport, PA facility   ph 610-916-3939
Charlie Waltman  ph 484-248-0466
Dan Cosma  ph 484-248-0401

Use the test procedure below.  Measurements should exceed 100k Ohms.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.