Browse FAQs

What are the replacement SCRs for the RAM DBS II?

Published date: 29 June 2020

Issue:
Replacement of SCRs for the RAM DBS II?
 
Product Line:
DBS and DBS II
 
Environment:
All models
 
Cause:
Replacement
 
Resolution:
Replacement SCRs are not offered as a repair part.  If an SCR has failed, either replace the entire DBS chassis or send the chassis to Schneider Electric Leesport for repair.
Either way, contact Indicon Corp

Please note that the DBS and DBS II product lines were sold to Indicon Corp.
Technical support contacts:
Leesport, PA facility   ph 610-916-3939
Charlie Waltman  ph 484-248-0466
Dan Cosma  ph 484-248-0401
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.