Browse FAQs

Can both an auxiliary switch and a shunt trip be installed in H-frame breaker?

Published date: 28 June 2018

Product Line:
Powerpact H and J frame

Resolution:
Yes. a maximum of two auxiliary switches (OF1 and OF2), one trip indication (SD), one fault-trip indication (SDE) and one remote-tripping release, either shunt trip (MX) or undervoltage trip (MN) can be installed in either a Powerpact H or J frame breaker.



 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.