Browse FAQs

Can I use a single phase input soft starter to power a three phase motor?

Published date: 19 May 2020

Issue:
Use a single phase input soft start with a three phase motor.

Product Line:
Altistart product.

Environment:
All models, All serial numbers

Cause:
Information unavailable in current literature.

Resolution:
No, A soft starter is not capable of generating a third phase.  A Variable Frequency Drive will be needed for this depending on HP and voltage rating.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.