Browse FAQs

What would cause an EtyP fault on the ATV21 and ATV212 drives?

Published date: 29 June 2020

Issue:
Altivar 21/Altivar 212 EtyP Fault

Product Line:
Altivar 21/Altivar 212

Environment:
All serial numbers for Altivar 21/Altivar 212

Cause:
N/A

Resolution:

• Set parameter [Parameter reset] (tYP) to 6.
• If this does not clear the detected error, replace the drive.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.