Browse FAQs

What is the Terminal Lug Data for the EZM1600FSB and the EZM1800FSB Main Devices?

Published date: 10 June 2020

Issue:
Standard Terminal Lug Data

Product Line:
EZM Metering

Environment:
EZM Molded Case Switch lugs

Cause:
Application

Resolution:
The Molded Case Switch used in EZM1600FSB and EZM1800FSB is the PowerPact M-Frame and the standard lug is AL800M23K and will accept as standard;
(3) 3/0-500kcmil Al/Cu wires per Phase(or per pole of the molded case switch) and the Main Neutral on these devices will accept as standard (4) 3/0-500kcmil Al/Cu wires (See the below attached CAD drawing).
 

Alternate lugs for Molded Case Switch used in the above catalog numbers:
1) Lug kit AL1200P24K will accept (4) 3/0-500kcmil Al/Cu wires. (1 lug per kit)
2) Lug kit AL800P6k will accept (2) 3/0 - 600kcmil Al/Cu wires. (3 lugs per kit)
3) Lut kit AL800P7K will accept (2) 3/0 - 750kcmil(BUT the 750kcmil wire MUST be Compact Aluminum wire ONLY. (3 lugs per kit)

Alternate lugs for the Main Neutral used in the above catalog numbers:
1) Lug kit MMLK250 will accept as standard (1) 1/0-600kcmil OR (2) 1/0-250kcmil Al/Cu wires PER lug. Kit includes (3)2-Barrel lugs and neutral will accommodate ONLY 2 lugs.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.