Browse FAQs

What is the Terminal Lug Data for the EZM31000GCBE/JCBE and EZM31200GCBE/JCBE Main Devices?

Published date: 10 June 2020

Issue:
Standard Terminal Lug Data

Product Line:
EZM Metering

Environment:
EZM Main Breaker lugs

Cause:
Application

Resolution:
The EZM31000GCBE, EZM31000JCBE, EZM312000GCBE, and EZM31200JCE are designed to meet the West Coast 'EUSERC' Utilities requirements and do not come standard with lugs from the factory, but contain Lug Landing Pads to meet the EUSERC requirements. Each Lug Landing pad on these catalog numbers will ONLY accommodate (3) lugs per pad (or 3 lugs per phase/neutral). This means these EZM main devices will ONLY accommodate (3) wires Per Phase/Neutral. See the below attached CAD drawing showing the part numbers of the lugs and the maximum wire size the lugs will accept. 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.