Browse FAQs

Can ANY of the Individual Circuit Breaker Enclosures(B, H, Q, QO, J, L, M or P frames) be mounted Horizontally or Pad mounted?

Published date: 03 June 2020

Issue:
Product Design Features 

Product Line:
Circuit Breaker Enclosures

Environment:
Installation

Cause:
Application

Resolution:
ALL of the circuit breaker enclosures are designed, tested and listed to ONLY be mounted Veritically and NOT Horizontally. Any other orientation would be between the installer and local code authority.

Also, the circuit breaker enclosures are designed to be wall mounted, they are not designed to be Pad Mounted or Floor mounted. 


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.