Browse FAQs

Are the Altivar 650 and Altivar 950 Process Drives available?

Published date: 19 June 2020

Issue:
How do I order an Altivar 650 (ATV650) or Altivar 950 (ATV950) drive?

Product Line:
Altivar Process Drive (ATV650, ATV950)

Environment:
All serial numbers for Altivar 650 and 950 Process Drive 

Cause:
N/A

Resolution:
Altivar 650
This drive is now available to order.  

In the past ATV630........ EU was the part number used in place of the ATV650.....EU drives.    The only difference is the ATV630....... EU has a Black color disconnect and the ATV650...... EU has a Red color disconnect. 

Altivar 950
These drives are not available for ordering yet.
To order a Nema 12 drive:
 - Order an Altivar 960 Enclosed drive using Product Selector with Nema 12 option. (For End Users/Customers please your contact local distributor for assistance)
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.