Browse FAQs

Which error class is triggered with a Sercos error on a LXM32S?

Published date: 07 August 2018

Issue:
Which error class (0,1,2,3 or 4) is triggered with a Sercos error on a LXM32S?
Can we define the error class like we do with other LXM32 drives?

Product:
LXM32S

Resolution:
The LXM32S does not use the DriveCom profile so you cannot specify the error class when a Sercos communication error happens.
The LXM32S uses a special control and status word and only supports the modes CSP, CSV or CST.
If there's a communication problem, the errors can be found in the list E Bxxx.
For general error handling in the application, you can use the Softmotion PLCopen function blocks in SoMachine.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.