Browse FAQs

What does restart pending mean in the MPPT60-150 status screen?

Published date: 25 June 2018

Issue:
MPPT60-150 where it states restart pending

Product Line:
MPPT60-150

Environment:
Installations that use renewable energy and a Schneider Electric MPPT60-150

Cause:
MPPT60-150 shows restart pending

Resolution:
The XW SCC is ready to restart but waiting for the timeout period to expire. This condition is normally only observed at dusk and dawn.  If you see this condition during peak times, please ensure you are getting the proper Voltage and Current from array.  Perform a power cycle by:
- Turning off FIRST PV breaker THEN the battery breaker.
- Turn on FIRST Battery Breaker, THEN PV breaker
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.