Browse FAQs

Getting alarm A324 on LXM32 drive

Published date: 29 June 2020

Issue:
Getting alarm A324 on the LXM32 drive

Product Line:
Lexium 32
LXM32

Resolution:
A324 is an error during the homing sequence of the LXM32
Possible reasons are a bad insulation on the limit switch wire, EMC interference caused by running a power cable next to the limit switch wire, a reference switch not enabled, low or no voltage on the reference or limit switches or multiple positive/negative/reference switches active

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.