Browse FAQs

How to Setup MV-90 to Read Primary or Secondary Data

Published date: 08 June 2020

Product Line
MV-90

Environment
Channel Master File in MV-90

Cause
The parameter that controls whether the MV-90 is reading primary or secondary values is Meter Multiplier.

Resolution
Set this parameter to:
  • 1: if the meter is set up to return primary data
  • (PT ratio) * (CT ratio):  if the meter is set up to return secondary data

Note: In order to find out if the meter is returning primary or secondary values refer to FA306381.

For complete information on how to setup MV-90 refer to MV-90 and ION Technology technical note.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.