Browse FAQs

How to Determine if an ION Meter is Returning Primary or Secondary Values

Published date: 08 June 2020

Issue
The meter owner wants to transfer secondary parameters to another software such as MV-90.

Product Line
ION Meter

Environment
ION Meter Template

Cause
The parameter that controls whether the meter is presenting primary or secondary values is Scale Rev Param.  This parameter is an External Boolean Module and used as an input in Scaling Arithmetic Module.

ION Setup can be used to control the parameter as shown here:



Resolution
Set Scale Rev Param parameter to:

ON: if primary values are to be presented
OFF: if secondary values are to be presented

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.