Browse FAQs

What are the differences in PME 8.1 Data Center and Standard editions?

Published date: 09 June 2020

Issue
Are there any differences in the Data center edition and the Standard edition of PME?

Product Line
Power monitoring Expert 8.1

Environment
Power monitoring

Cause
 The standard and data center versions of PME are very similar. With the introduction of PME 8.1 it is possible to build a data center solution from the standard PME edition including all of the same modules

Resolution


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.