{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What are the repair parts for the CHU363AWC, series F7 (may be shown as F07)?

Issue:
Replacement parts

Product Line:
Safety Switches

Resolution:
The repair parts for the CHU363AWC, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056775250 (includes all poles; arc suppressor assembly not included)
-Line Base Mounting Screw - 4020515101(3 required)
-Arc Suppressor Assembly - 4056635550 (1 required)
-Arc Suppressor Mounting Screw - 4020514501
-Lug Assembly - 4025101851 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Lockplate - 4056672101
-Lockplate Mounting Screw - 2299940562 (2 required)
-Handle Assembly - 4056663550 (also recommend replacing handle assembly external gasket)
-Handle Assembly External Gasket - 4056603101
-Switch Mechanism - 4056787350 (also requires switch mechanism washer and interlock gasket; handle assembly external gasket may also need replacing)
-Switch Mechanism Washer - 2360200008
-Interlock Gasket - 4056786001
-Rod/Linkage Assembly - 4056787150
-Receptacle - 2541002295
-Receptacle Mounting Screws - 4510280101 (4 required)
-Ground Lug - 4025101851 (3 required)
-Ground Lug Mounting Screw - 4020514801 (long screw) and 4020513503 (short screw)

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.